Leopard Imaging ToF Cameras

Time-of-Flight (ToF) Cameras

Leopard Imaging’s Sirius Time-of-Flight Cameras

Redefining Time-of-Flight Camera Technology

The basic working principle behind a ToF camera is the time light takes to bounce off an object. The time taken is then processed and the distance between all objects in a scene is determined. Leopard Imaging’s ToF cameras use this data for three-dimensional object mapping, effectively recreating a scene and calculating different parameters such as depth, distance, etc.

Often referred to as ‘depth cameras’, our robust ToF camera systems offer the best-in-class performance while consuming less computing power. This enables power-efficient ToF camera systems to be deployed on a mass scale.
A proud member of the NVIDIA Partner Network, Leopard Imaging focuses on developing ToF cameras for imaging solutions that are compatible with the NVIDIA Jetson AGX Xavier platform. We offer hardware and software development as well as fine-tuning services for both developers and customers.

Developed in exclusive collaboration with NVIDIA, our ToF camera systems are also listed in Jetson AGX Orin and Thor. This productive collaboration allows us to empower several industries such as IoT, automotive visual applications, robotics, deep learning, visualization, and edge IT.

Time of Flight Technology Overview

A ToF camera measures how long it takes for light to bounce off an object. Using this principle, the camera calculates the distance to all objects in a scene. This point cloud data is used to compute and create a three-dimensional (3D) map of the object space. Thus, ToF cameras are also referred to as “depth cameras.” Unlike stereo 3D methods, no image contrast is necessary, and ToF systems exhibit excellent mechanical robustness.

Sirius Plus Dual RGB + iToF Perception System

The LI-OG05B20-AF0130-GMSL2-085H Sirius Plus is a powerful dual-sensor perception platform that combines the onsemi® AF0130 indirect Time-of-Flight (iToF) sensor with the OMNIVISION® OG05B20 global shutter RGB sensor to deliver synchronized depth and color imaging in a compact GMSL2 camera system. Designed for robotics, intelligent automation, and advanced machine vision applications, Sirius Plus provides accurate real-time depth sensing, enhanced environmental awareness, and reliable RGB-D data for AI-driven perception, navigation, and object detection in dynamic operating environments.

Sirius Max Next-Generation RGB-D Perception

The LI-AR0234-AF0130-TX10-GMSL2-140H Sirius Max is an advanced RGB-D perception platform engineered for robotics, industrial automation, and autonomous navigation. Combining high-performance RGB imaging, intelligent indirect Time-of-Flight (iToF) depth sensing, embedded processing, and Lumotive’s programmable beam-steered illumination, Sirius Max delivers long-range active depth perception and real-time RGB-depth fusion within a fully integrated GMSL2 camera system. Designed to power next-generation AI perception, it enables enhanced environmental awareness, object detection, and navigation performance in demanding real-world applications.

Applications & Industries

Retail
Physical Security
Healthcare
Drones
IOT
Robotics
Automotive
industry 4.0

Questions?

Contact Us

What is a Time-of-Flight (ToF) camera?

A ToF camera is an advanced imaging device that measures the time it takes for light to bounce off objects in a scene, creating depth maps and 3D representations of the environment.

How do ToF cameras work?

ToF cameras emit light pulses and measure the time taken for the light to return after reflecting off objects. This time measurement is used to calculate distances, creating a detailed 3D map of the surroundings.

What are the advantages of ToF cameras?

ToF cameras offer several key advantages:

  1. High-speed 3D imaging, capable of frame rates up to 60 fps or higher.
  2. Operate in various lighting conditions, including low-light environments.
  3. Provide accurate depth information with resolutions up to 1 MP (megapixel).
  4. Consume less computing power, typically requiring only 1-2W for operation.
  5. Compact size, often less than 100mm x 100mm for industrial models.
  6. Wide field of view, commonly ranging from 60° to 90°.
  7. Ability to capture depth information for multiple objects simultaneously.

    How accurate are ToF cameras?

    Modern ToF cameras can achieve millimeter-level accuracy in ideal conditions, though real-world accuracy may vary based on environmental factors and the specific camera model.

    What is ToF used for?

    ToF technology has diverse applications:

    1. 3D mapping and environment reconstruction with centimeter-level accuracy.
    2. Object detection and tracking in real-time, processing up to 60 frames per second.
    3. Gesture recognition for touchless interfaces, detecting movements as subtle as finger twitches.
    4. Augmented reality for precise object placement within 1-2mm accuracy.
    5. Autonomous navigation, providing depth information up to 10 meters away.
    6. Facial recognition, capturing 3D facial features with sub-millimeter precision.
    7. Volume measurement in logistics, accurate to within 1-2% of actual volume.

    What applications benefit from ToF technology?

    ToF cameras benefit numerous industries and applications:

    1. Robotics: Obstacle avoidance and object manipulation with millimeter precision.
    2. Automotive: ADAS systems, utilizing ToF for pedestrian detection up to 200 feet away.
    3. Retail analytics: Customer tracking and heat mapping with 98% accuracy.
    4. Physical security: Intruder detection in low-light conditions, effective up to 20 meters.
    5. Healthcare imaging: Non-invasive body measurements accurate to within 0.5cm.
    6. Drone navigation: Collision avoidance systems reacting within milliseconds.
    7. IoT devices: Smart home sensors for occupancy detection and energy management.

    How do ToF cameras compare with LiDAR systems?

    While both provide 3D sensing, ToF cameras are generally more compact, power-efficient, and cost-effective.